Annotation Options

Configuration Instructions

Cross section annotation displays information about the cables and conductors contained within the conduit. In the example below the annotation displays the ObjectID (28968), Conductor Material (Aluminum), Conductor Size (2 AWG) and Phase (ABC) field values of the conductor associated with the conduit. The numbers at the beginning of each line (1, 4, 6) correspond with the ducts in which the phases of the conductor reside. 

This section discusses the various methods for configuring the Cross Section Annotation contents list.

Cross section annotation with a leader line.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.