Tasks

Process Framework tasks can be executed on specific events during the post process. While configuring the post process, right-click an event and select Add Task.

Set the Action Name field to any value that's meaningful. The Process Framework Task field must match the name of the task as it is configured in the database EXACTLY. To view a list of tasks in your Process Framework database, use the Process Framework Administration tool. Tasks are listed on the Node Types tab.

You can assign an existing task to multiple events. To do this, right-click the existing task and click Copy. Right-click an event and select Paste. 

To remove a task, right-click it and select Delete Task.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.