Is Standard Design?

Checks to see if the selected design is enabled for Designer (and not Designer Express). This subtask determines the design type using the product family type table.

Enabled

  • Selected node must be a design.

  • MMWorkflowManager must be the current extension.

Execute

  • Always returns true. 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.