Restore All Backup Packets

Pulls all packets from the transporter's backup folder and restores them to the working directory.

Enabled

  • The database must support Mobile.

  • Packets must exist in the transporter's backup folder.

Execute

  • Pulls all packets from the backup folder and places them in the working directory.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.