ESENT File Cleanup in Geodatabase Manager

Geodatabase Manager deletes all the ESENT files (.edb files) created in AppData\Roaming\Miner and Miner, whenever the Feeder Sync action handler finishes its processing of a version. Microsoft ESENT and Local Storage includes more information on ESENT files.

The cleanup action removes only those files that have reached the age limit configured for Feeder Manager 2's cleanup activity for ESENT files, provided that the files are not still being used by the service. The intent is to prevent the accumulation of a large number of .edb files, rather than ensure the instant removal of every .edb file that appears.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.