Does User Own Work Request or Design Node?

Checks to see if the user is also the current owner.

Enabled

  • If the user is not the owner, the Enabled method returns false and the subtask is disabled.

Execute

  • Always returns true.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.