Change Session Owner Self

Changes the owner of the selected node to the current user.

Enabled

  • MMSessionManager must be the current extension.

  • Determines if there are any other users that have a role that can access the node in its current state.

Execute

  • Changes the owner of the node to the current user.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.