Configure Design Optimization

Design Optimization simplifies the design process by using administrator-defined parameters to automatically place the optimal features for your layout. Your administrator may elect to provide multiple design type parameters. Each set of parameters may be tailored toward a specific type of design.

Secondary Circuit Analysis must be configured before configuring Design Optimization.

Optional Configurations

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.