Update Enterprise

Uses the Database ID to update the enterprise with mobile packets from the user working directories on the enterprise.

Enabled

  • A Database ID value must exist in the field database.

Execute

  1. Removes packets from the user's transporter directory based on the Database ID.

  2. Uses the Database ID to place the packets in the appropriate enterprise working directory.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.