Send Session

Identifies whether the user is in the field or on the enterprise and executes the appropriate task: Send Session to Enterprise or Send Session to Field.

Enabled

  • A valid PxNode must have been passed into this subtask.

  • That PxNode must be a session node.

  • Field: The "Send Session to Field" task must be enabled.

  • Enterprise: The "Send Session to Enterprise" task must be enabled.

Execute

  1. Checks to see if the user is in the field or on the enterprise.

  2. If the user is in the field, executes Send to Enterprise task.

  3. If the user is on the enterprise, executes the Send to Field task.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.