Is Session Locked?

Checks the session to determine if it is locked.

Enabled

  • Disabled if the session’s node is locked.

  • Disabled if the session has a packet and Mobile is disabled.

  • MMSessionManager must be the current extension.

  • The selected node is a session node.

Execute

  • Always returns true.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.