Voltage Regulator

Object Model names: None

Field Model names:

Field

Field Model Name

Properties

FeederID

FEEDERID

Field Info Tab:

Reset After Create = Yes

FeederID2

FEEDERID2

Field Info Tab:

Reset After Create = Yes

FeederInfo

FEEDERINFO

Field Info Tab:

Editable = No

Reset After Create = Yes

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

Field Info Tab:

Reset After Create = Yes

PhaseDesignation

PHASEDESIGNATION

 

RatedKVA

RATEDKVA

 

Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network.

ParentCircuitSourceGUID

PARENTCIRCUITSOURCEGUID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

PARENTCIRCUITSOURCEID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

FacilityID

FACILITYID

Field Info Tab:

Visible = Yes

Editable = Yes

Reset After Create = No

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.