All Feature Classes in the Geometric Network

Assign the following autoupdaters to every feature class that participates in the geometric network. Many classes have autoupdaters that will replace these. However, every feature class in the network should have autoupdaters assigned to the On Feature Create and On Feature Update events.

Extended Feeder Manager: If you're configuring Extended Feeder Manager, do not assign the ArcFM Create Feeder Object and ArcFM Update Feeder Object autoupdaters on features you want to act as subsources. 

Event

Autoupdater

On Feature Create

ArcFM Create Feeder Object

On Feature Update

ArcFM Update Feeder Object

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.