Duct Size Options

Configuration Instructions

Once the Duct Size Options have been configured, users may place ducts within ducts in ArcFM.

To place ducts within ducts, it is necessary to have a field in the duct definition object class with a model name of DUCTSIZE. This field model name is used to determine at what size ducts are plotted in map units (or another unit of measure; see note). The duct size field may be assigned a custom editor that restricts the values of the size field so users cannot select a duct that is equal to or larger than the master duct.

TIP: You can set the unit of measure for ducts using the ArcFM Properties Manager. Right-click the geodatabase and select ArcFM Properties Manager. Choose the Underground Facilities tab.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.