Add Model Names

Before assigning model names and field model names, you must ensure they have been created.

Add the following class model names to the Electric Object Class Model Name domain:

  • CIRCUITSOURCE
  • DYNAMICPROTECTIVEDEVICE
  • ELECTRICNETWORKEDGE
  • FDRMGRLOADPOINT
  • FDRMGRNONTRACEABLE
  • FDRMGRPROTECTIVE
  • FEEDERSECONDARY
  • OPENPOINT
  • SPLITTARGET
  • SWITCH
  • TRANSFORMER
  • TRANSFORMERUNIT (optional: used to show RatedkVA)

Optional: The following model names are required only if you have a multi-tiered network and Extended Feeder Manager.

  •   CIRCUITSOURCEID

Add the following field model names to the Electric Field Model Name domain:

  • FEEDERID
  • FEEDERID2
  • FEEDERINFO
  • FDRMGRNONTRACEABLE
  • FEEDERNAME
  • FEEDERSOURCEINFO
  • LOWSIDEVOLTAGE
  • MMELECTRICTRACEWEIGHT
  • NORMALPOSITION_A
  • NORMALPOSITION_B
  • NORMALPOSITION_C
  • OPERATINGVOLTAGE
  • PHASEDESIGNATION
  • RATEDKVA (optional: used to show RatedkVA)
  • SUBSTATIONID

Optional: The following field model names are required only if you have a multi-tiered network and Extended Feeder Manager.

  • CIRCUITSOURCEGLOBALID
  • CIRCUITSOURCEGUID
  • CIRCUITSOURCEID
  • FACILITYID
  • FEEDERLEVEL
  • PARENTCIRCUITSOURCEGUID
  • PARENTCIRCUITSOURCEID 
  • RELATEDFEATURECLASSNAME
  • RELATEDOBJECTID
  • SUBSOURCE
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.