Upgrade to Extended Feeder Manager

If you maintain a multi-tiered network, but do not have Feeder Manager configured, follow all of the steps on the Overview page and include the portions marked "Optional" with each step.

Perform this upgrade ONLY if your situation meets the following criteria:

  • You maintain a multi-tiered network

  • You have an existing configuration of Feeder Manager

Follow the steps below to upgrade your existing configuration to use Extended Feeder Manager.

Step 1: Create Domains

Step 2: Add Fields

Step 3: Create CircuitSourceID Table

Step 4: Add Model Names to Domains

Step 5: Assign Model Names

Step 6: Assign Autoupdaters

Step 7: Define Subsources

Step 8: Define Ultimate Sources

Step 9: Jigger Ultimate Sources

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.