Process Framework Subtasks

Below is a list of the subtasks you can use with Process Framework extensions (e.g., Session Manager, Workflow Manager), the criteria necessary for you to be able to enable them, and the steps the application performs when it executes them. Many of these subtasks are named after their associated task.

You may also create custom subtasks.

Use the Process Framework Admin Tool to group subtasks and create custom tasks.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.