Prepare Database and Create Domains

Prepare your database

Right-click your database in ArcCatalog and run both of the following tools:

  •  Upgrade ArcFM Solution Database

  •  Create/Upgrade ArcFM System Tables

Create Domains

Apply the following domain properties to each domain listed below.

  • Field Type: Long Integer
  • Domain Type: Coded Values
  • Split policy: Duplicate
  • Merge policy: Default Value

FdrMgrNonTraceable

If you plan to create a FdrMgrNonTraceable field on one or more of your edge feature classes, create a domain to be applied to fields carrying the FDRMGRNONTRACEABLE field model name (assigned in a future step).

Code

Description

0

Traceable

1

NonTraceable

NormalStatus

This domain provides values for the possible positions of switchable devices.

Code

Description

0

Open

1

Closed

2

Not Applicable

Phase Designation

Phasing allows you to maintain information on individual phases of a conductor or device.

Code

Description

1

C

2

B

3

BC

4

A

5

AC

6

AB

7

ABC

Single Phase

This domain provides phasing for single-phase conductors and devices.

Code

Description

1

C

2

B

4

A

Two Phase

This domain provides phasing for two-phase conductors and devices.

Code

Description

3

BC

5

AC

6

AB

Three Phase

This domain provides phasing for three-phase conductors and devices.

Code

Description

7

ABC

Transformer Unit kVA

The ArcFM Electric Trace Options includes an option to display kVA by phase for a trace. To access this option in ArcMap, click the Options button on the ArcFM Electric Traces toolbar and select the Electric Traces tab:

With this option checked, the Rated kVA dialog is shown after each trace. This displays the sum of the Rated kVA (by phase) for all transformer units returned by the trace. If transformer units are not present, the rated kVA is calculated from the kVA values of the transformers. If it's not configured, or configured incorrectly, it displays values of 0.0.

To display Rated kVA for a trace, you must create the following domain. This domain holds the possible Rated kVA values in your network. The following table shows an example of how you might create this domain. Your domain will probably have more values.

Code

Description

10

10 kVA

15

15 kVA

25

25 kVA

38

37.5 kVA

50

50 kVA

75

75 kVA

100

100 kVA

YesNo

This domain is used for numerous fields across the ArcFM Solution.

Code

Description

0

No

1

Yes

Create Model Name Domains

If they do not already exist, create and populate the domains that contain the electric field and object class model names. Apply the following domain properties to each domain listed below.

Field Type: Text

Domain Type: Coded Values

Split policy: Default Value

Merge policy: Default Value

Electric Field Model Name

Populate this domain with all of the following field model names.

Code

Description

CIRCUITSOURCEID

CIRCUITSOURCEID

FDRMGRGANGOPERATED

FDRMGRGANGOPERATED

FDRMGRNONTRACEABLE

FDRMGRNONTRACEABLE

FACILITYID

FACILITYID

FEEDERID

FEEDERID

FEEDERLEVEL

FEEDERLEVEL

FEEDERNAME

FEEDERNAME

LOWSIDEVOLTAGE

LOWSIDEVOLTAGE

MMELECTRICTRACEWEIGHT

MMELECTRICTRACEWEIGHT

NORMALPOSITION_A

NORMALPOSITION_A

NORMALPOSITION_B

NORMALPOSITION_B

NORMALPOSITION_C

NORMALPOSITION_C

OPERATINGVOLTAGE

OPERATINGVOLTAGE

PHASEDESIGNATION

PHASEDESIGNATION

RATEDKVA

RATEDKVA

SUBSOURCE

SUBSOURCE

SUBSTATIONID

SUBSTATIONID

Electric Object Class Model Name

Populate this domain with all of the following object class model names.

Code

Description

CIRCUITSOURCE

CIRCUITSOURCE

CIRCUITSOURCEID

CIRCUITSOURCEID

DYNAMICPROTECTIVEDEVICE

DYNAMICPROTECTIVEDEVICE

ELECTRICNETWORKEDGE

ELECTRICNETWORKEDGE

FDRMGRLOADPOINT

FDRMGRLOADPOINT

FDRMGRNONTRACEABLE

FDRMGRNONTRACEABLE

FDRMGRPROTECTIVE

FDRMGRPROTECTIVE

FEEDERSECONDARY

FEEDERSECONDARY

OPENPOINT

OPENPOINT

PROTECTIVE

PROTECTIVE

SPLITTARGET

SPLITTARGET

SWITCH

SWITCH

TRANSFORMER

TRANSFORMER

TRANSFORMERUNIT

TRANSFORMERUNIT

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.