2601_MTN6705-0008S_MTN6805-0008_SW

Slat Position after Movement

With every blind movement, the position of the slats also changes, depending on the direction of motion. After the movement, the slats stay in this new position. With this application, however, you can automatically move or reset the slats to a desired position after a movement.

Using the parameter “Slat position after movement”, you can define the behavior of the slats after a movement for each blind channel.

The following parameters are available for this:

  • No reaction (stay in the current position)

  • Operating position (move to operating position)

  • Last slat position (move to the slat opening angle that the blind had before the start of the movement)

The slat opening angle you have defined is set after each positioning movement of the blind or after a manual motion command terminated by a stop telegram.

After a bus voltage failure or a download, the last slat position is not clearly defined, so the last slat position is assumed to be the operating position.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?