2601_MTN6705-0008S_MTN6805-0008_SW

Priority

The scene function has the same priority as the normal switching function via the “switch object”. This should be taken into account with regard to the priority of the higher-level functions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?