2601_MTN6705-0008S_MTN6805-0008_SW

Group Objects for Switch Counter

If you enable the Switch counter, group objects for each relay appear in the special object folder Switching cycle counter.

No.

Name

Object function

Length

Behavior

Data Type

31 – 38

Master Output #

Switching cycle counter

2 bytes

Sends/Reads

2 byte unsigned value

39 – 46

Extension 1 Output #

Switching cycle counter

2 bytes

Sends/Reads

2 byte unsigned value

47 – 54

Extension 2 Output #

Switching cycle counter

2 bytes

Sends/Reads

2 byte unsigned value

By default only C-Flag and R-Flag are set to avoid high bus traffic.

The firmware checks the internal counters cyclically every 10 seconds. If the value changes, it is sent via the group object.

You can read the actual values via group objects. If you want to get to know the values without reading, you have to set the T-Flag for the object.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?