2601_MTN6705-0008S_MTN6805-0008_SW

Name of the Channel for Switching

You can assign a separate name for each channel, e.g. “Light Hall Ground Floor”. This individual name is appended to the fixed channel name, e.g., “Master Output 1 - Switch”. The full name of the channel is then “Master Output 1 - Switch Light Hall Ground Floor”.

The name of the channel now appears on the parameters, channels and associated group objects.

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Express settings for switching

 
 

Name of the channel

Light Hall Ground Floor

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?