2601_MTN6705-0008S_MTN6805-0008_SW

Idle Time until Upward Movement

If the blind used has an idle time in the closed lower position between pulling on the main strap and the first upward movement, you can compensate for this delay in this way.

The idle time can also be used when using a roller shutter to compensate for the roller shutter opening.


Example:

A value = 10 gives an idle time of 10 x 10 ms = 100 ms

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Extended drive timing

-Extended drive timing

Idle time until upward movement (0...255, unit = 10 ms)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?