2601_MTN6705-0008S_MTN6805-0008_SW

Group Objects for Failure Indicator

No.

Name

Object function

Length

Behavior

Data Type

27

Master

Fault - Internal

1 bit

Sending

1.001 Switch

28

Master

Fault - External

1 bit

Sending

1.001 Switch

The Fault – Internal object signals internal device faults detected during the self-test. The Schneider-Electric Device Firmware Update Tool can be used to diagnose the fault with the integrated diagnostics function.

The Fault – External object signals external installation faults. The Schneider-Electric Device Firmware Update Tool can be used to diagnose the fault with the integrated diagnostics function.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?