2601_MTN6705-0008S_MTN6805-0008_SW

Blinking Interval

The blinking speed is set here. A blinking interval (on/off) can be set between 5 and 60 seconds.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?