2601_MTN6705-0008S_MTN6805-0008_SW

Proportion Open/Closed

You can parameterize the ratio between closed and open relay during a blinking time.

You can select whether the relay is to be open/closed equally (Equal) during a blinking interval (50%/50%) or short open/long closed (20% / 80%) or long open/short closed (80%/20%).


Proportion open/closed

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?