2601_MTN6705-0008S_MTN6805-0008_SW

Behavior after Defined Number of Blinking Intervals

You can specify the state to which the relay will be switched after the defined number of blinking intervals.

Either Relay is closed or Relay is opened.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?