2601_MTN6705-0008S_MTN6805-0008_SW

Staircase Lighting Time Function (Staircase Timer)

This function is used to switch on an appliance, e.g., the light in a staircase, via a bus telegram and automatically switch it off again after a set duration. Therefore, no manually or automatically generated bus telegram is required for switching off. The actuator carries out the switching off operation independently and under time control.

Two types of staircase lighting time function are available:

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Staircase lighting time

 
– Time settings

Staircase lighting time

Disabled

Fix

Variable

Following enabling of the corresponding staircase lighting time function, the relevant group object appears.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?