2601_MTN6705-0008S_MTN6805-0008_SW

Enable Central Function for Each Drive

The central function is enabled or disabled here for each drive.

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind / roller shutter

Express settings for blind / roller shutter

Scenes settings

Central function

Enabled

Disabled

The global settings and explanations of the central function can be found in the chapter General settings (Enabling Central Functions).

Using the central function, you can simultaneously open or close multiple blind channels with a telegram via the object Central – Move up/down blind.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?