2601_MTN6705-0008S_MTN6805-0008_SW

Setting the Blind Type (for Blind only)

If you wish to program the slat control for a blind, you should define your blind type before starting the parameterization.

The application distinguishes between four different types of blinds, which you can recognize by the position of their slats during the movement. Two of these types have a mechanically defined operating position. They can be recognized seen from the tilted slat position during a downward movement. The operating position limits the possible opening angle of the slats, unless the blind is in its lower end position.

This is done using the parameter Movement of the existing blind.

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

Blind

Express settings for blind

 

Slat control

 

Movement of the existing blind

Downwards closed / upwards horizontal

 

Downwards tilted / upwards horizontal

     

Downwards closed / upwards closed

     

Downwards tilted / upwards closed

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?