2601_MTN6705-0008S_MTN6805-0008_SW

Blinking

The switching mode Blinking alternately opens and closes the relay. You can define the blinking behavior for each channel. The blinking speed is defined using the parameter Blinking interval. The blinking cycle starts with a closed relay.

Furthermore, you can set the ratio between closed and open relay during a blinking time in 3 steps. You can reduce the blinking intervals to a defined number to protect the relay. Additionally, you can specify the state to which the relay will be switched after the defined number of blinking intervals.


IMPORTANT: Short switching times must not be parameterized under load (see technical data of the switching output).

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Express settings for switching

 

Switching mode

Blinking

Behavior at pressed/released

Blinking / relay opened

Blinking / relay closed

Relay opened / blinking

Relay closed / blinking

 

Blinking interval

5 s

(5 s - 60 s)

 

Proportion open/closed

Equal (50/50%)

Short open / long closed (20/80%)

Long open / short closed (80/20%)

 

Defined number of blinking intervals (0...255, 0 = permanent blinking)

20

   

Behavior after defined number of blinking intervals

Relay is closed

Relay is opened

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?