2601_MTN6705-0008S_MTN6805-0008_SW

Priority

The alarm function is a 1-bit group object with high priority. The device safety function has the highest priority.

The priority order for blind / roller shutter can be defined globally Priority of Functions for Roller Shutter and Blind. The alarm object takes precedence over the following group objects:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?