Selection of the SpaceLogic KNX Extensions
The SpaceLogic KNX Switch/Blind Master is a KNX actuator that switches a maximum of 8 outputs (such as lamps) or controls a maximum of 4 blind motors with end switches. The distribution of functions between channels is freely selectable and depends on your requirements.
If you need more channels for your project, you can connect so-called SpaceLogic KNX Switch/Blind extensions to the master. As with the master, channels can be split into switching channels or blind channels. Since a master can control a maximum of 2 extensions, it is possible to switch a maximum of 24 outputs or control a maximum of 12 blind motors.
|
General settings |
Selection of the SpaceLogic KNX extension |
||
|
Type of Extension 1 |
Disabled |
||
|
MTN6805-0008 Switch/Blind |
|||
|
Type of Extension 2 |
Disabled |
||
|
MTN6805-0008 Switch/Blind |
|||
Selecting MTN6805-0008 Switch/Blind adds Extension 1. The 8 new outputs with tabs, parameters, channels and channel functions are now available in the application.
Selecting MTN6805-0008 Switch/Blind as Extension 2 adds the second Switch/Blind extension.
For Extension 2, the new outputs are now displayed with tabs, parameters, channels and channel functions.