2601_MTN6705-0008S_MTN6805-0008_SW

Lock Behavior after Download

After a download, the lock function is also set as in the case of bus voltage recovery. The parameter "Behavior after download" determines which state is set.

If the "Behavior after download" parameter is set to "As before download", the locking function is activated as previously set and the relay is switched accordingly.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?