2601_MTN6705-0008S_MTN6805-0008_SW

Status of Height

The current position of the drive is provided as a value between 0-100%. The corresponding status object “Feedback for height” sends the value on the bus if the drive has reached a fixed position after a movement.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?