2601_MTN6705-0008S_MTN6805-0008_SW

Staircase Lighting Time Fix

With Staircase lighting time fix, you can parameterize a fixed staircase lighting time for each channel. The staircase lighting time can be parameterized between 5 seconds and 1 hour. This function makes the Staircase fix object (1 bit) available to you.

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Staircase lighting time fix

 
– Time settings

Manual switching off

Active

Not active

 

Time extension

Not retriggerable

Retriggerable

Retriggerable and adding

   

Max. number of additions

2 (2 - 5)

   

Duration time

2 min (5 s - 1 h)

 

Number of prewarnings

0 (0 - 5)

 

Warning starts (5...255, unit = 1s) before end

20 (5 - 255)

   

Hint: Staircase duration time must be longer or equal than prewarning start time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?