2601_MTN6705-0008S_MTN6805-0008_SW

Pause Time before Reverting (Pause on Reverse)

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

Blind/roller shutter

Express settings for blind/roller shutter

 

Blind control / roller shutter control

 

Pause time before reverting (2...255, unit = 100 ms)

5

If the channel for a drive that is currently in motion receives a motion command in the opposite direction, it first turns off both output relays for this channel.

Before turning on the relay for the new direction of motion, it waits for the set Pause time before reverting.

The channel observes the pause on reverse even if it is to rotate the slats in different directions when executing two step commands (for blind only).


NOTICE
The drive may be damaged.
The drive may be damaged if the pause times are too short. Be sure to refer to the specifications in the data sheet of the drive manufacturer when setting the values.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?