2601_MTN6705-0008S_MTN6805-0008_SW

OR Logic Operation

As long as the "logic object" has the value "0", switching can be carried out as usual using the address of the "switch object". Set staircase times continue to be observed. Switching on via the "logic object" takes effect immediately.

Object Logical input

Object Switching

Result

0

0

0

0

1

1

1

0

1

1

1

1

Example:

An OR logic operation can be used to implement a power-off lock or Central ON function (e.g. light for cleaning buildings). If the value of the "switch object" is also set to "1" locally, the relay remains switched on when the power-off lock is withdrawn (value change of logic object from 1 to 0).


OR logic operation;
Value of logic object after bus voltage recovery: 0


OR logic operation;
Value of logic object after bus voltage recovery: 1

The logic object is preset to the value "1" after a RESET. The actuator will switch on the output immediately. The OR logic function is only reset by a "0" telegram on the logic object.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?