2601_MTN6705-0008S_MTN6805-0008_SW

Relay Behavior after Bus Voltage Recovery

In the case of bus voltage recovery, the relay can adopt a parameterized state.


Possible settings:

Pressed:
In the case of a normally opened contact, the relay is closed; in the case of a normally closed contact, the relay is opened.


Released:
In the case of a normally opened contact, the relay is opened; in the case of a normally closed contact, the relay is closed.


As before bus voltage failure:
With the parameter “As before bus voltage failure”, the relay adopts the state that was saved in the device at the time of the bus voltage failure. Any subsequent manual switchings are overwritten.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?