2601_MTN6705-0008S_MTN6805-0008_SW

Group Objects of Automatic Mode for Blind/Roller Shutter

No.

Name

Object function

Length

Behavior

Data Type

60

Master Output 1+2 name of the channel

Movement in automatic mode

1 bit

Received

1.008 Up/Down

61

Master Output 1+2 name of the channel

Stop/step in automatic mode (blind)

1 bit

Received

1.007 Step

61

Master Output 1+2 name of the channel

Stop in automatic mode (roller shutter)

1 bit

Received

1.007 Step

62

Master Output 1+2 name of the channel

Height position in automatic mode

1 byte

Received

5.001 Percent (0...100%)

63

Master Output 1+2 name of the channel

Slat position in automatic mode (blind)

1 byte

Received

5.001 Percent (0...100%)

The group objects for manual operation and automatic mode have equal priority. The drive always executes the command it received last on one of the objects.

Using parameter settings and objects, you can modify the operation of the two control options. You also have the possibility of defining the reciprocal influence of manual control and automatic control.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?