2601_MTN6705-0008S_MTN6805-0008_SW

Calling and Saving Scene Values

Scene values for the output relays are called using the object “Scene”. After receiving a scene telegram, the device evaluates the sent scene address and controls the channels to the saved scene values.

If a reference movement is required before the drive is moved to the scene position, the reference movement is executed first and the drive then moves to the requested scene position.

Calibration

If the “scene object” receives a scene telegram with learning bit “1”, then for all scenes assigned to the received scene address, the current height position and, in the case of blind drives, the current slat position are saved as the new scene value.


NOTE: Note: If a scene address within a channel is assigned to multiple scenes (incorrect parameterization), only the last scene found with this scene address is called or saved. You can avoid this by assigning different scene addresses within a channel.


Telegram format

Telegrams for the scene function have the data format: L X D D D D D D.

L = learning bit

X = not used

DDDDDD = called scene address

If the learning bit in a telegram has the value “0”, then the relay states saved for the scene address are called and set.

If the learning bit receives the value “1”, then the current output states are saved as new scene values for the received scene address.

Take the scene address (0-63) and add 128 to get the value for learning the scene.


Examples:

Telegram value

Binary

Hexadecimal

Scene address

0

0000 0000

00

Call scene address 0

1

0000 0001

01

Call scene address 1

29

0001 1101

1D

Call scene address 29

57

0011 1001

39

Call scene address 57

63

0011 1111

3F

Call scene address 63

128 (0+128)

1000 0000

80

Learning scene address 0

129 (1+128)

1000 0001

81

Learning scene address 1

157 (29+128)

1001 1101

9D

Learning scene address 29

185 (57+128)

1011 1001

B9

Learning scene address 57

191 (63+128)

1011 1111

BF

Learning scene address 63

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?