2601_MTN6705-0008S_MTN6805-0008_SW

Number of Scenes

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Scene settings

 

Scenes settings

Required number of scenes

1 (1 – 16)

You can use the scene function to include multiple channels in a scene control. Up to 16 different scenes are available for each output channel.

Each of the 16 scenes can be disabled again.

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Scene settings

 

Scenes settings

Scene 1 (1-16)

Disabled

Enabled

   

Scene 1 Description

   

Scene 1 Address (0-63)

Dependent: Global Settings for Scenes

Scene address 0 - 63

   

Scene 1 Address (1-64)

Dependent: Global Settings for Scenes

Scene address 1 - 64

   

Scene 1 switching state

Released

Pressed

For clarity, a short description can be stored for each scene.

Each of these scenes can be assigned one of 64 possible scene addresses 0 to 63 (corresponding to telegram values 0-63) or 1 to 64 (corresponding to telegram values 0-63). This depends on the global settings for scenes.

Global Settings for Scenes


You can store the switching states (pressed, released) as scene values for each output channel.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?