2601_MTN6705-0008S_MTN6805-0008_SW

Roller Shutter Control Drive Time

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

Express settings for roller shutter

 

Roller shutter control

   

Use same time for up and down

Yes

   

Running time: Up/Down (5s...99:59.9 min)

02:00.0

   

Pause time before reverting (2...255, unit = 100 ms)

5

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

Express settings for roller shutter

 

Roller shutter control

   

Use same time for up and down

No

     
   

Running time: Up (5s...99:59.9 min)

02:00.0

   

Running time: Down (5s...99:59.9 min)

02:00.0

   

Pause time before reverting (2...255, unit = 100 ms)

5

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?