2601_MTN6705-0008S_MTN6805-0008_SW

Roller Shutter

To control roller shutter, you can switch the channel function of the device to Roller shutter mode.

General settings

Channel function Master / Extension 1 / Extension 2 Output 1-8 Roller shutter
   

Master/Ext. 1/2
Output 1-8 – Roller shutter: Roller shutter

Express settings for Roller shutter

...

Express Settings for Roller Shutter

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?