2601_MTN6705-0008S_MTN6805-0008_SW

Enable Scene Learning

The parameter Enable learning of scenes is activated as standard and the learning of scenes is thus allowed. This can be disabled globally.

Extended settings

Global settings for scene

 

Enable learning of scenes

Yes

     

No

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?