2601_MTN6705-0008S_MTN6805-0008_SW

On-delay

Master/Ext. 1/2 Output 1-8 -Switch: Switching

On-delay time

 
– Time settings

On-delay time

Enabled

Disabled

   

Works on Switch object

Yes (Yes/No)

   

Works on Staircase object

No (Yes/No)

   

Works on Scene object

No (Yes/No)

   

On-delay mode

Not retriggerable

Retriggerable

   

On-delay time

1 s (0 ms-1 h)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?