2601_MTN6705-0008S_MTN6805-0008_SW

Locking Manual Mode

Locking Manual Mode

Master / Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

Express settings for roller shutter

   

Locking manual mode

Disabled

Enabled

   

Manual locking

At object value "1"

At object value "0"

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?