2601_MTN6705-0008S_MTN6805-0008_SW

Functions with Higher Priority

The order of priority of the various functions is set on the Extended settings tab of the device.

Priority of Functions for Switching

In the ETS, the higher priority function can be activated.

Master/Ext. 1/2 Output 1-8 -Switch: Switching

Priority function

 
– Logic, Locking & Priority settings

Higher priority function

Disabled

Priority function

Locking function

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?