2601_MTN6705-0008S_MTN6805-0008_SW

Behavior at the End of Locking

If the locking function has been switched off again by a new object value, you can operate the drive normally again. If the drive is to perform an automatic action after the locking function has been terminated, you can define it with this parameter:

  • No reaction: the drive remains in its current position.

  • Up: the drive moves to the upper end position.

  • Down: the drive moves to the lower end position.

  • Move to position prior locking: the drive returns to the position it had before the locking.

  • Accept current automatic position: this setting is only useful if the automatic function is active. The drive moves to the last automatic position requested.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?