2601_MTN6705-0008S_MTN6805-0008_SW

Priority of Functions for Roller Shutter and Blind

The global priorities for roller shutter and blind are defined here. The safety function has the highest priority. The other priorities can be selected here.

Extended settings

Global settings for roller shutter and blind

  Priority of functions Safety > Alarm > Weather alarms > Lock > All other
 

Safety > Alarm > Lock > Weather alarms > All other

 

Safety > Weather alarms > Alarm > Lock > All other

   

Safety > Weather alarms > Lock > Alarm > All other

   

Safety > Lock > Alarm > Weather alarms > All other

     

Safety > Lock > Weather alarms > Alarm > All other

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?